Boot Loader required LPC2124

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boot Loader required LPC2124

2,376 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by basavaraja_br on Mon Jan 19 00:06:09 MST 2015
Dear All
we are facing again some issue in  LPC2124FBD64/01 which as BOOT LOADER ID-1.65  version; IC (LPC2124) with  BOOT LOADER ID-1.70   is OK fine with application software.

I have Below link to get the new boot loader, but it is not opening ; kindly help

http://www.nxp.com/files/products/standard/microcontrollers/utilities/lpc2000_bl_update.zip


Thanks
BR
Labels (1)
0 Kudos
Reply
2 Replies

2,282 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by basavaraja_br on Tue Jan 20 20:36:24 MST 2015
Hi,
Thanks for the response.. above link provides bootloader version 1.63 which is older than existing 1.65 where we have the problem; hence

We are looking for Boot loader version 1.70, which work well with our application software..

kindly helps us!!

Thanks
Basavaraja.B.R
0 Kudos
Reply

2,282 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by djonesboni on Tue Jan 20 06:07:42 MST 2015
Google: lpc2000_bl_update ext:zip

Found a Google Code link .../p/semestre6/source/browse/trunk/SE2/DOCS/LPC2000/lpc2000_bl_update.zip

In the right click on View raw file.

Be careful, this may not be the file you want.

:)
0 Kudos
Reply