Boot LPC4330 from SPI/SSP: what chips are supported?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Boot LPC4330 from SPI/SSP: what chips are supported?

2,335件の閲覧回数
gertvierman
Contributor II

I just found out that the LQFP144 package can only mux the I2S1 through the same pins which are needed for the SPIFI, which I currently use to boot.

Alternative would be to boot from SPI/SSP instead of SPIFI. Does anyone have experience with this, and what SSP/SPI chips are know to be compatible with the LPC43xx boot rom?

Thanks,

4 返答(返信)

2,212件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Gert,

We don't currently have a list of supported SPI flash devices, we have only tested QSPI. Compatability should be good with a wide range of SPI devices because SPI boot operates at a much lower speed.


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信

2,212件の閲覧回数
gertvierman
Contributor II

AT45DB161E boots successfully.

2,212件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Gert,

 

It is good to hear that! thanks for letting us know.

 

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信

2,212件の閲覧回数
gertvierman
Contributor II

Ok, thank you. I planned for the Atmel AT45DB161E on my board, I'll share my results here when I tested.