Bluetooth integration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bluetooth integration

3,646件の閲覧回数
vxs187
Contributor III

I have setup a bluetooth module to capture data from the LPC through an Arduino. I see a lot of data getting lost, could someone tell me if there is a bluetooth library for nxp's lpc4370? 

ラベル(1)
タグ(2)
5 返答(返信)

3,522件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Visweshwar Srinivasan,

I contacted wireless team, there is no bluetooth library for lpc4370.

NXP has bluetooth solution for these wireless chips:

Bluetooth®Smart/Bluetooth Low Energy|NXP 


Have a great day,
Jun Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,522件の閲覧回数
vxs187
Contributor III

Hi Zhang Jennie, 

There is no Bluetooth module in the LPC4370, but I am sure I can integrate the MC with a HC05, is UART the only solution? 

Thanks!

0 件の賞賛
返信

3,522件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Visweshwar Srinivasan,

What do you mean "integrate the MC with a HC05, is UART the only solution? " ?

Can you please be more specific?

Jennie Zhang

0 件の賞賛
返信

3,522件の閲覧回数
vxs187
Contributor III

So I need to transfer data from my nxp microcontroller using UART communication. Could you tell me if that's possible? I have been trying to communicate and have not been able to do so this far, is there an example I could refer? 

0 件の賞賛
返信

3,522件の閲覧回数
BlackNight
NXP Employee
NXP Employee