Blinky load fails

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Blinky load fails

2,414件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gurlavie on Mon Apr 25 13:50:41 MST 2016
Hi,

Sorry for probably posting the most stupid of the posts ever, but eventually after days and days of trying, I need some helps :(
I got my LPCXpresso LPC1115 Rev A unit.

Trying to run Periph_Blinky.

- When connecting the unit to Power, I get Led2 blinking.
- Then I compile and "debug" "Periph_Blinky" Project.

No matter what I do, I get an error "15: Target error from Commit Flash write"

Reading the error description, I thought it is a power issue for the flash writing.
- I used a power USB HUB - still same issue
- I moved to a docking station connectivity - still same issue

Still nothing - I always get the error, and then Led2 stops blinking.

Maybe I am doing something much more basically wrong ?
Is Periph_Blinky compatible to 1115 ?

Any suggestion on how to go forward ?

Thanks

Gur
ラベル(1)
0 件の賞賛
返信
6 返答(返信)

2,397件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信

2,397件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gurlavie on Sat Apr 30 13:21:46 MST 2016
With the right project it works perfectly ! thanks !
0 件の賞賛
返信

2,397件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gurlavie on Mon Apr 25 22:08:46 MST 2016
Thanks !

Downloaded and testing. Will report back on the status. Thanks for the help !
0 件の賞賛
返信

2,397件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Mon Apr 25 20:28:07 MST 2016

Quote: gurlavie
Or better, which one (and where to get) the one I need for the 1115 ?



http://www.lpcware.com/system/files/lpcopen_v2_00a_lpcxpresso_nxp_lpcxpresso_11c24.zip  :O  :quest:  :D

as described in:

https://www.lpcware.com/content/nxpfile/lpcopen-software-development-platform-lpc11xx-packages-0


Quote:
LPCXpresso LPC11C24 board

[color=#f00]Supports LPC11[/color]11/12/13/14/[color=#f00]15[/color]/00XL

0 件の賞賛
返信

2,397件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gurlavie on Mon Apr 25 16:15:08 MST 2016
I thought I followed the orders in the guide to get it.

How do I validate the package I use ?
Or better, which one (and where to get) the one I need for the 1115 ?

tx!
0 件の賞賛
返信

2,397件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Apr 25 15:22:01 MST 2016

Are you confident which board you have? The periph_blinky project is included in various LPCOpen packages. Which LPCOpen package are you using?

Thanks and regards,
LPCXpresso Support
0 件の賞賛
返信