Bit field descriptions for the Protected Flash Region

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bit field descriptions for the Protected Flash Region

Jump to solution
6,127 Views
gvellet
Contributor II

Hi,

In the LPC55S69 user manual UM11126 page 252, it is written "Note: For bit field descriptions, see the attached Protected Flash Region.xls for further details."  Where can I find this excel file?

In the MCUXpresso Secure Provisioning tool, some information is given for the bitfield but it is not detailed.

For instance, in the location CMPA:SPI_FLASH_CFG, the bit field "SPI_RECOVERY_BOOT_EN" is 5-bit with no explanation. In the user manual, the same bitfield is said to have only 4-bit. Obviously the protected Flash bit fields are updated faster than the user manual.

Perhaps for designers with NXP device experience, most of these details are obvious. But for a new comer like me, I stumble a lot trying to understand this device.

Thanks

Labels (1)
0 Kudos
Reply
1 Solution
5,953 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @gvellet 

I'm sorry for the inconvenient to you. I have submitted request to add this.

I send you the Rev.2.5 for reference. Please see my attachment. Thanks.

 

BR

Alice

View solution in original post

4 Replies
6,076 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @gvellet 

Please open the attachment in UM11126, you will find the "Protected Flash Region.xls". As below:

Alice_Yang_0-1719916196875.png

 

Please contact us if still have any issue.

 

BR

Alice

 

0 Kudos
Reply
6,030 Views
gvellet
Contributor II
The attachment is no longer in the latest PDF release. See my Tuesday july 2nd reply for details
0 Kudos
Reply
5,953 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @gvellet 

I'm sorry for the inconvenient to you. I have submitted request to add this.

I send you the Rev.2.5 for reference. Please see my attachment. Thanks.

 

BR

Alice

6,065 Views
gvellet
Contributor II

Hi Alice,

In the current UM11126 file, there is no attachment. Can you attached the xls file to this message thread?

gvellet_0-1719928129704.png

Thanks,

Gilbert Vellet

0 Kudos
Reply