Best way to check amount data received through the DMA

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Best way to check amount data received through the DMA

553 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by philw4321 on Mon Feb 02 14:26:32 MST 2015
Hi,

I am using the DMA to receive data from the USUART port. I am trying to figure out the best way to check the amount (number bytes) of data I actually received at the end of the time out period. I do use the DMA interrupt to indicate when a fixed amount of data has been received, the length I request is sometimes larger than the amount of data actually received. The data is real just less than the requested amount from the DMA.

So I am looking to figure out how much data I did receive when I do not get an interrupt.

I there a mechanism to check the DMA pnt position?

For reference I am using FreeRTOS with task notification for the time out and this is the setup of the DMA transfer:


    TransferStaus = Chip_GPDMA_Transfer(LPC_GPDMA,
dmaChannelNumRx,
_GPDMA_CONN_UART2_Rx,
&pucRxData[0],
GPDMA_TRANSFERTYPE_P2M_CONTROLLER_DMA,
(uint32_t) uiRxLength);

Many Thanks,

Phil
标签 (1)
0 项奖励
回复
0 回复数