Batch updating of project properties?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Batch updating of project properties?

626 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wheels on Fri Apr 01 15:29:03 MST 2016
My company is developing a new board based on the 1778. It's similar enough to the 1788 that we can start with the LPCOpen library for the EA_Devkit board. We've got our first article boards in, and I'm trying to set up a couple of workspaces for different configurations of it (one standard, one specific to an individual customer). I've used the rename capability to change the "lpc_board_ea_devkit_1788" project to a different name, and I've updated the files in there for our hardware.

My problem is that all of the other projects that I imported still refer to the EA board in their include paths, libraries, and library path properties, in both the Debug and Release configurations. Do I have to change these one at a time, or is there some way to update them all simultaneously?
Labels (1)
0 Kudos
Reply
1 Reply

615 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply