Basic SPI Communication Workflow

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Basic SPI Communication Workflow

1,523 Views
easter91
Contributor I

Hi there,

i am using a LPC1788 on the EmbeddedArtists Eval Board and would like to communicate other devices via SPI.

After including the lpc177x_8x_ssp library i am using the following code to initialise :

SSP_CFG_Type SSP_ConfigStruct;
SSP_ConfigStruct.CPHA = SSP_CPHA_FIRST;
SSP_ConfigStruct.CPOL = SSP_CPOL_HI;
SSP_ConfigStruct.ClockRate = 1000000;
SSP_ConfigStruct.Mode = SSP_MASTER_MODE;
SSP_ConfigStruct.FrameFormat = SSP_FRAME_SPI;
SSP_ConfigStruct.Databit = SSP_DATABIT_8;

SSP_Init(LPC_SSP0,&SSP_ConfigStruct);
SSP_Cmd(LPC_SSP0,ENABLE);

In the main loop i try to do :

SSP_SendData(LPC_SSP0,0x05);

Using  a scope i can not see any pulses on the clock line.

What am i missing here ? Can someone point out the basic syntax to read and write a register from/to a SPI-device for me ?

Labels (2)
Tags (3)
0 Kudos
Reply
1 Reply

1,330 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi  Christian Ostermeier,

    Please test the lpcopen code for Embeddedartists eval LPC1788 board directly.

  You can download the lpcopen code from this link:

LPCOpen Software for LPC17XX|NXP 

After it works on your board, you can refer to that code to modify it.

I find you didn't initialize the SPI pin at least.

Wish it helps you!

Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply