BOD reset level

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

BOD reset level

跳至解决方案
2,158 次查看
peterwöß-krausb
Contributor I

Hello,

table 21 in the datasheet LPC11U6x / Rev. 1.3. shows the characteristics for the 

interrupt level 2 & 3, and for reset level 2 & 3.

What are the characteristics for reset level 0 & 1, as table 58 / document UM10732 

allows BOD reset level 0, 1, 2, 3.

Best regards, 

Peter

标签 (1)
0 项奖励
回复
1 解答
1,976 次查看
soledad
NXP Employee
NXP Employee

Hi Peter,

On the LPC11U6x, those levels are not there since the assertion points are below the minimum operating Vdd voltage.

 only levels mentioned in the datasheet are workable thresholds available.

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,977 次查看
soledad
NXP Employee
NXP Employee

Hi Peter,

On the LPC11U6x, those levels are not there since the assertion points are below the minimum operating Vdd voltage.

 only levels mentioned in the datasheet are workable thresholds available.

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,976 次查看
peterwöß-krausb
Contributor I

thx

0 项奖励
回复