BGA256: What's pin D8 ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BGA256: What's pin D8 ?

1,272件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Pacman on Sun Nov 04 18:19:39 MST 2012
I can't find Pin D8 in the datasheet for the BGA256 package.
Pin B8 is listed as NC, but what about pin D8, is it a secret ? =)

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,261件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Pacman on Sun Nov 04 23:16:11 MST 2012
Heh. Very appropriate. Thank you very much! :)

Oh, BTW: I made a mistake above - B9 is not connected, not B8...

As a small thank-you, you can play around with this toy if you want...

http://arm.gpio.dk/lpc43xx.html
0 件の賞賛
返信

1,261件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by DF9DQ on Sun Nov 04 21:31:13 MST 2012
WAKEUP3
0 件の賞賛
返信