Availability of CAN bus in small packages

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Availability of CAN bus in small packages

983 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MichelKuenemann on Thu Apr 16 04:52:23 MST 2015
Hi NXP,

I am fond of NXP  Cortex Mx microcontrollers (like LPC824, LPC11C24, LPC1549, LPC1769, LPC4330) which are all very good products.

I plan to design an industrial miniature smart sensor and I need a CAN interface. I have spent a lot of time searching an NXP M0 or M3 controller in a small package (TSSOP 16/20 HVQFN33 or even WLCSP) in vain. The smallest footprint currently available for CAN bus enabled NXP microcontrollers seems to be the QFP48 (LPC11C24 or LPC154X).

So my question: is there a plan at NXP to release M0/M3 controllers with CAN buses in very small packages (LPC = Low Pin Count !)

Thank you.
Regards,
Michel Kuenemann
标签 (1)
0 项奖励
回复
2 回复数

948 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MichelKuenemann on Thu Apr 16 07:19:53 MST 2015
How could I guess that Save = Post ?
0 项奖励
回复

948 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Thu Apr 16 06:40:25 MST 2015
Don't multiple post!
0 项奖励
回复