Audio Output Device example for LPC43XX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Audio Output Device example for LPC43XX

1,714件の閲覧回数
k2
Contributor III

Audio Output Device example for LPC43XX. Can someone point me to a USB Device Speaker example for the LPC43XX family ? I'm trying out a Hi-Def DAC with a 4357. I found an example for the 54608 family, is there one for the LPC43XX family ?

ラベル(3)
0 件の賞賛
返信
1 返信

1,595件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello  Kevin King,

You can have a look at this thread:

Audio Output Device example  

the example you can find from: 

nxpUSBlib v0.98.zip  


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信