Audio Class code generation not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Audio Class code generation not working

2,653 Views
asca
Contributor I

Greetings,

I'm using the MCUXpresso version 24.12 with the LPC5526 SDK version for USB stack 2.11.0.

When I try to configure the USBHSD interface for Audio control and streaming, I get the following error: "Issue: "USB device audio" driver is missing in the project." However this component IS included in the SDK and enabled in the SDK manager. The peripheral is also enabled but the code cannot be generated because of this error.

Please see the screenshots in the attachement and the .mex config file.

This happens regardles of the audio interface version (both on 1.0 and 2.0).

What could be the possible cause of this issue?

Labels (2)
0 Kudos
Reply
2 Replies

2,464 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi  

I created a new LPC5526 project under IDE 24.12 and SDK 25.03. I didn't see error. How to reproduce the error?

ZhangJennie_1-1748425682934.png

 

ZhangJennie_0-1748425430796.png

Thanks,

Jun Zhang

0 Kudos
Reply

2,489 Views
domtom555
Contributor I

Hi,

I have the same problem, did you solve it by any chance?

BR

0 Kudos
Reply