Atollic configuration missing in LPC54xxx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Atollic configuration missing in LPC54xxx

1,736 Views
Catosh
Contributor IV

Hello, 

I downloaded the SDK V2.0 for LPC5411x derivatives but in the toolchain folders there are only MDK and IAR.
Do I need to select some specific configuration do have all the toolchains present or True Studio is not supported by the SDK?

B.R.

Luca

Labels (1)
Tags (3)
0 Kudos
Reply
2 Replies

1,581 Views
soledad
NXP Employee
NXP Employee

Hi,

The SDK 2.0.0 was compiled and tested only with these development tools:
• LPCXpresso 8.2.0
• IAR Embedded Workbench for ARM® platform version7.60.2
• MDK-ARM Microcontroller Development Kit (Keil)®5.20

Sorry for any inconvenience that may cause.


Have a great day,

Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,581 Views
Catosh
Contributor IV

Hello Soledad, thanks for you reply. 
No inconvenience, I saw the picture in the user guide and thought I was missing some point!
B.R.

Luca.

0 Kudos
Reply