Are there any USB HID example for LPC1768?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Are there any USB HID example for LPC1768?

1,255 次查看
yan_m
Contributor I

I just found this: LPCOpen Software for LPC17XX | NXP

But these examples are for LPC1788 and LPC1769.

Does anyone know where I can find an example?

标记 (2)
0 项奖励
回复
1 回复

1,210 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

HI

There is no example for LPC1768, please use LPCopen for LPC1769 for your device instead.

The only difference between LPC1768 and 1769 is max CPU speed. LPC1768 is 100MHz; LPC1769 is 120MHz.

Have a great day,
Jun Zhang

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复