Arduino code on LPC1347

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Arduino code on LPC1347

4,414件の閲覧回数
nidalp
Contributor I

Anyone interested running Arduino (generic) code, or using Arduino libraries (like Adafruit) on LPC13xx (or almost any other LPC), check this out: Arduino-XC - LPC1347

Very usable (UART, SPI, I2C, half a dozen of Adafruit libraries: ADXL345, BMP085, GFX/LCD, ST7735, TCS34725, LSM303) but still under heavy development.

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

2,956件の閲覧回数
nidalp
Contributor I

Here is a short video of LPCXpresso 1347 board running code from Arduino IDE.

Compiler and uploader are from LPCXpresso IDE installed on the same workstation. This is proof of concept which uses libraries that come with Arduino-XC (SPI, Serial, Wire, some Adafruit libs etc.).

Serial Monitor seems to have some issues with FTDI USB serial dongle I'm using, so I just used minicom to display serial data coming from the board.

0 件の賞賛
返信