Arduino code on LPC1347

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Arduino code on LPC1347

4,305 次查看
nidalp
Contributor II

Anyone interested running Arduino (generic) code, or using Arduino libraries (like Adafruit) on LPC13xx (or almost any other LPC), check this out: Arduino-XC - LPC1347

Very usable (UART, SPI, I2C, half a dozen of Adafruit libraries: ADXL345, BMP085, GFX/LCD, ST7735, TCS34725, LSM303) but still under heavy development.

标签 (2)
标记 (1)
0 项奖励
回复
1 回复

2,847 次查看
nidalp
Contributor II

Here is a short video of LPCXpresso 1347 board running code from Arduino IDE.

Compiler and uploader are from LPCXpresso IDE installed on the same workstation. This is proof of concept which uses libraries that come with Arduino-XC (SPI, Serial, Wire, some Adafruit libs etc.).

Serial Monitor seems to have some issues with FTDI USB serial dongle I'm using, so I just used minicom to display serial data coming from the board.

0 项奖励
回复