Any idea how to enable and download in external ram?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Any idea how to enable and download in external ram?

1,362 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by goffi on Fri Jun 14 01:50:16 MST 2013

I have a dev board from embedded artists with lpc4357.


I'm trying to enable the external ram (with iar+jlink) and download the program on it.


In my .mac file i put these lines but i have problems on the commented parts:


//SystemInit


 


//MemoryPinInit


__writeMemory32(0x000000f3, 0x4008609c, "Memory" );


__writeMemory32(0x000000f3, 0x400860a0, "Memory" );


__writeMemory32(0x000000f3, 0x400860a4, "Memory" );


__writeMemory32(0x000000f3, 0x400860a8, "Memory" );


__writeMemory32(0x000000f3, 0x400860ac, "Memory" );


__writeMemory32(0x000000f3, 0x400860b0, "Memory" );


__writeMemory32(0x000000f3, 0x400860b4, "Memory" );


__writeMemory32(0x000000f3, 0x400860b8, "Memory" );


__writeMemory32(0x000000f2, 0x40086290, "Memory" );


__writeMemory32(0x000000f2, 0x40086294, "Memory" );


__writeMemory32(0x000000f2, 0x40086298, "Memory" );


__writeMemory32(0x000000f2, 0x4008629c, "Memory" );


__writeMemory32(0x000000f2, 0x40086280, "Memory" );


__writeMemory32(0x000000f2, 0x40086284, "Memory" );


__writeMemory32(0x000000f2, 0x40086288, "Memory" );


__writeMemory32(0x000000f2, 0x4008628c, "Memory" );


__writeMemory32(0x000000f2, 0x40086688, "Memory" );


__writeMemory32(0x000000f2, 0x4008668c, "Memory" );


__writeMemory32(0x000000f2, 0x40086690, "Memory" );


__writeMemory32(0x000000f2, 0x40086694, "Memory" );


__writeMemory32(0x000000f2, 0x40086698, "Memory" );


__writeMemory32(0x000000f2, 0x4008669c, "Memory" );


__writeMemory32(0x000000f2, 0x400866a0, "Memory" );


__writeMemory32(0x000000f2, 0x400866a4, "Memory" );


__writeMemory32(0x000000f3, 0x40086714, "Memory" );


__writeMemory32(0x000000f3, 0x40086718, "Memory" );


__writeMemory32(0x000000f3, 0x4008671c, "Memory" );


__writeMemory32(0x000000f3, 0x40086720, "Memory" );


__writeMemory32(0x000000f3, 0x40086724, "Memory" );


__writeMemory32(0x000000f3, 0x40086728, "Memory" );


__writeMemory32(0x000000f3, 0x4008672c, "Memory" );


__writeMemory32(0x000000f3, 0x40086730, "Memory" );


__writeMemory32(0x000000f3, 0x40086124, "Memory" );


__writeMemory32(0x000000f3, 0x40086128, "Memory" );


__writeMemory32(0x000000f3, 0x4008612c, "Memory" );


__writeMemory32(0x000000f3, 0x40086130, "Memory" );


__writeMemory32(0x000000f3, 0x40086134, "Memory" );


__writeMemory32(0x000000f2, 0x40086080, "Memory" );


__writeMemory32(0x000000f2, 0x40086084, "Memory" );


__writeMemory32(0x000000f2, 0x40086088, "Memory" );


__writeMemory32(0x000000f3, 0x40086120, "Memory" );


__writeMemory32(0x000000f3, 0x4008611c, "Memory" );


__writeMemory32(0x000000f2, 0x40086118, "Memory" );


__writeMemory32(0x000000f2, 0x40086108, "Memory" );


__writeMemory32(0x000000f2, 0x40086104, "Memory" );


__writeMemory32(0x000000f2, 0x40086100, "Memory" );


__writeMemory32(0x000000f1, 0x40086320, "Memory" );


__writeMemory32(0x000000f1, 0x4008631c, "Memory" );


__writeMemory32(0x000000f2, 0x400866c0, "Memory" );


__writeMemory32(0x000000f2, 0x400866bc, "Memory" );


__writeMemory32(0x000000f3, 0x40086700, "Memory" );


__writeMemory32(0x000000f3, 0x40086704, "Memory" );


__writeMemory32(0x000000f3, 0x40086708, "Memory" );


__writeMemory32(0x000000f3, 0x4008670c, "Memory" );


__writeMemory32(0x000000f3, 0x40086710, "Memory" );


__writeMemory32(0x000000f3, 0x40086510, "Memory" );


__writeMemory32(0x000000f3, 0x40086090, "Memory" );


__writeMemory32(0x000000f1, 0x40086318, "Memory" );


__writeMemory32(0x000000f2, 0x400866b4, "Memory" );


__writeMemory32(0x000000f2, 0x400866a8, "Memory" );


__writeMemory32(0x000000f3, 0x40086324, "Memory" );


__writeMemory32(0x000000f3, 0x40086098, "Memory" );


__writeMemory32(0x000000f3, 0x40086310, "Memory" );


__writeMemory32(0x000000f3, 0x40086314, "Memory" );


__writeMemory32(0x000000f3, 0x4008632c, "Memory" );


__writeMemory32(0x000000f3, 0x40086330, "Memory" );


__writeMemory32(0x000000f3, 0x40086328, "Memory" );


__writeMemory32(0x000000f2, 0x40086680, "Memory" );


__writeMemory32(0x000000f3, 0x40086734, "Memory" );


__writeMemory32(0x000000f3, 0x4008608c, "Memory" );


__writeMemory32(0x000000f3, 0x40086090, "Memory" );


__writeMemory32(0x000000f3, 0x40086094, "Memory" );


__writeMemory32(0x000000f3, 0x40086098, "Memory" );


 


//EMCFlashInit


__writeMemory32(0xc28f5c29, 0x4000520c, "Memory" );


__writeMemory32(0xc28f5c29, 0x40005210, "Memory" );


__writeMemory32(0x00000001, 0x40005000, "Memory" );


__writeMemory32(0x00000081, 0x40005200, "Memory" );


__writeMemory32(0xc28f5c29, 0x40005208, "Memory" );


__writeMemory32(0x00080000, 0x40005200, "Memory" );


 


//CGU_Init


__var temp;


 


//CGU_SetXTALOSC


temp = __readMemory32( 0x40050018, "Memory" );


temp = temp & 0xfffffffb;


__writeMemory32( temp, 0x40050018, "Memory" );


 


//CGU_EnableEntity


temp = __readMemory32( 0x40050018, "Memory" );


temp = temp & 0xfffffffe;


__writeMemory32( temp, 0x40050018, "Memory" );


 


//CGU_EntityConnect


//temp = __readMemory32( 0x40053630, "Memory" );


//temp = (temp & 0xf0ffffff) | 0x06000000 | 0x00000800;


//__writeMemory32( temp, 0x40053630, "Memory" );


//__writeMemory32( 0x06000803, 0x40053630, "Memory" );


 


//CGU_SetPLL1


temp = __readMemory32( 0x40050044, "Memory" );


temp = (temp & 0xff00cc3d);


__writeMemory32( temp, 0x40050044, "Memory" );


 


temp = __readMemory32( 0x40050044, "Memory" );


temp = temp | 0x00050140;


__writeMemory32( temp, 0x40050044, "Memory" );


 


//CGU_EnableEntity


temp = __readMemory32( 0x40050044, "Memory" );


temp = temp & 0xfffffffe;


__writeMemory32( temp, 0x40050044, "Memory" );


 


//while(40050040) == 0


 


//CGU_EntityConnect


//temp = __readMemory32( 0x40055610, "Memory" );


//temp = (temp & 0xf0ffffff)| 0x09000000 | 0x00000800;


//__writeMemory32( temp, 0x40055610, "Memory" );


__writeMemory32( 0x09000800, 0x40055610, "Memory" );


 


 


//CGU_SetPLL0


temp = __readMemory32( 0x40050020, "Memory" );


temp = temp | 0x00000001;


__writeMemory32( temp, 0x40050020, "Memory" );


 


__writeMemory32( 0x00202062, 0x40050028, "Memory" );


__writeMemory32( 0x04167ffa, 0x40050024, "Memory" );


__writeMemory32( 0x0600001c, 0x40050020, "Memory" );


 


//CGU_EnableEntity


temp = __readMemory32( 0x40050020, "Memory" );


temp = temp & 0xfffffffe;


__writeMemory32( temp, 0x40050020, "Memory" );


 


 


//CGU_EntityConnect


//temp = __readMemory32( 0x40054c80, "Memory" );


//temp = ( temp & 0xf0ffffff ) | 0x07000000 | 0x00000800;


//__writeMemory32( temp, 0x40054c80, "Memory" );


__writeMemory32( 0x07000800, 0x40054c80, "Memory" );


 


 


//CGU_EnableEntity


__writeMemory32( 0x00000010, 0x400860cc, "Memory" );


 


//CGU_EntityConnect


//temp = __readMemory32( 0x400562d0 );


//temp = ( temp & 0xf0ffffff ) | 0x03000000 | 0x00000800;


//__writeMemory32( temp, 0x400562d0, "Memory" );


__writeMemory32( 0x03000800, 0x400562d0, "Memory" );


 


 


//CGU_EnableEntity


 __writeMemory32( 0x00000013, 0x40086600, "Memory" );


 


//CGU_EntityConnect


//temp = __readMemory32( 0x40055fa0 );


//temp = ( temp & 0xf0ffffff ) | 0x02000000 | 0x00000800;


//__writeMemory32( temp, 0x40055fa0, "Memory" );


__writeMemory32( 0x02000800, 0x40055fa0, "Memory" );


 


 


//vEMC_InitSRDRAM


__writeMemory32(0x00005555, 0x40086d00, "Memory" );


__writeMemory32(0x00000001, 0x40005000, "Memory" );


__writeMemory32(0x00000000, 0x40005008, "Memory" );


__writeMemory32(0x00004700, 0x40005100, "Memory" );


__writeMemory32(0x00004700, 0x40005140, "Memory" );


__writeMemory32(0x00000303, 0x40005104, "Memory" );


__writeMemory32(0x00000303, 0x40005144, "Memory" );


__writeMemory32(0x00000001, 0x40005028, "Memory" );


__writeMemory32(0x00000002, 0x40005030, "Memory" );


__writeMemory32(0x00000005, 0x40005034, "Memory" );


__writeMemory32(0x00000008, 0x40005038, "Memory" );


__writeMemory32(0x00000001, 0x4000503c, "Memory" );


__writeMemory32(0x00000005, 0x40005040, "Memory" );


__writeMemory32(0x00000001, 0x40005044, "Memory" );


__writeMemory32(0x00000008, 0x40005048, "Memory" );


__writeMemory32(0x00000008, 0x4000504c, "Memory" );


__writeMemory32(0x00000008, 0x40005050, "Memory" );


__writeMemory32(0x00000001, 0x40005054, "Memory" );


__writeMemory32(0x00000001, 0x40005058, "Memory" );


__writeMemory32(0x00000183, 0x40005020, "Memory" );


__delay( 100 );


__writeMemory32(0x00000103, 0x40005020, "Memory" );


__writeMemory32(0x00000002, 0x40005024, "Memory" );


__delay( 100 );


__writeMemory32(0x00000076, 0x40005024, "Memory" );


__writeMemory32(0x00000083, 0x40005020, "Memory" );


__writeMemory32(0x00000000, 0x40005020, "Memory" );


__writeMemory32(0x00084700, 0x40005100, "Memory" );


__writeMemory32(0x00084700, 0x40005120, "Memory" );


__writeMemory32(0x00084700, 0x40005140, "Memory" );


__writeMemory32(0x00084700, 0x40005160, "Memory" );


<div>Any help is appreciate! Thanks</div>
Labels (1)
0 Kudos
Reply
2 Replies

1,134 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by goffi on Tue Jun 18 06:58:14 MST 2013

'll change it for iar. Many thanks for your help!!

0 Kudos
Reply

1,134 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bavarian on Tue Jun 18 01:32:27 MST 2013

Hello,


I attached two script files for KEIL µVision which work for the Hitex board (16-bit SDRAM) and the KEIL board (32-bit SDRAM). They are a little bit better commented than the IAR file you have, so maybe it helps.


The script file for the KEIL board should work for the embedded artists board as well, it seems to be a similar SDRAM type.


Regards,


NXP Technical Support

0 Kudos
Reply