An issue with adding an endpoint on the USB Audio journey of LPCXprosso55s69

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

An issue with adding an endpoint on the USB Audio journey of LPCXprosso55s69

1,783 Views
MHY_0878
Contributor I

Hello NXP developers, I recently used the LPCX presso 55s69 board official routine usb_device_composite_hid_audio_unified modify the code, the USB protocol stack I changed from 5 to 6, the USB enumeration passed, but the number of endpoints used is more than 4, the host can not send data to the microcontroller, I want to know why, please help me, thank you.

Labels (1)
0 Kudos
Reply
2 Replies

1,672 Views
MHY_0878
Contributor I
The problem has been solved. Thank you for your reply.
mhy
0 Kudos
Reply

1,746 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @MHY_0878 

LPC55S69 supports up to 16 endpoints.

And i checked your project.

Harry_Zhang_0-1736317636895.png

BR

Harry

0 Kudos
Reply