An issue with adding an endpoint on the USB Audio journey of LPCXprosso55s69

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

An issue with adding an endpoint on the USB Audio journey of LPCXprosso55s69

1,760件の閲覧回数
MHY_0878
Contributor I

Hello NXP developers, I recently used the LPCX presso 55s69 board official routine usb_device_composite_hid_audio_unified modify the code, the USB protocol stack I changed from 5 to 6, the USB enumeration passed, but the number of endpoints used is more than 4, the host can not send data to the microcontroller, I want to know why, please help me, thank you.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,649件の閲覧回数
MHY_0878
Contributor I
The problem has been solved. Thank you for your reply.
mhy
0 件の賞賛
返信

1,723件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @MHY_0878 

LPC55S69 supports up to 16 endpoints.

And i checked your project.

Harry_Zhang_0-1736317636895.png

BR

Harry

0 件の賞賛
返信