Adding SPI Hardware to OM13098

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Adding SPI Hardware to OM13098

1,886件の閲覧回数
anealca
Contributor II

What connector pins (J10,11,12?) can I to add an SPI DAC to the OM13098 development board without disabling any of the hardware on the board?

I think I can use Flexcomm 9.

ラベル(2)
0 件の賞賛
返信
1 返信

1,815件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Adrian Neal ,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
It's available to use two below sets of pins to connect an external SPI device, please give a try.

Pin Name   Board Location    
MISO          J9 pin 11         
MOSI          J9 pin 13        
PCS0          J9 pin 15         
SCK            J9 pin 9          

Pin Name  Board Location
MISO           J13  pin 12
MOSI           J13  pin 2
PCS0            J9   pin 3
 SCK             JP11 pin 2


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信