Adc Read Problem.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Adc Read Problem.

1,097 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sukrubahadir on Sat May 28 02:07:07 MST 2016
Hello,
I am trying to use adc peripheral.
I want to read 2 kHz sine wave with adc. Adc Clock is 12 Mhz. But when ı toggle the pin in the adc irq handler, this pin's frequency is 53 kHz.
This is unexpected behavior for me. Why this pin's freq is 53 kHz ?

Second, I am writing adc value to the dac value. I expect to see the adc signal in the dac output. But for example, when the 10 hz sine wave applied to the adc pin, dac output is look like the adc input signal. But when the frequency of the sine wave (adc input) is increased, dac output's peak to peak value is decreased. This is also unexpected behavior for me ?

Can you explain this unexpected behaviours ?

Thanks for your responses :)
Labels (1)
0 Kudos
Reply
1 Reply

1,050 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply