About usage of SPIFI in LPC18xx.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About usage of SPIFI in LPC18xx.

ソリューションへジャンプ
1,762件の閲覧回数
kalpeshramani
Contributor I

Hi,

I had developed application code based on SPIFI for "Spansion S25FL512S device".

Right now i want to know that, Can i use SPIFI driver for the device which is not actually memory but the output is same as it should be.

Let me explain,

I have one sensor which works as MASTER and it's output is 2 bit SPI(Works as Dual bit SPI Mode). Check attachment for more information on data lines.

Actually that sensor send data on(SPI D0, SPI D1) lines continuously in MASTER mode without any rest with reference clock. So Can i use SPIFI as slave in LPC1857 device to read that data?

Thanks in Advance.

Thanks,

Kalpesh Ramani.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,519件の閲覧回数
ckphua
NXP Employee
NXP Employee

The SPIFI interface can only be used a Master only. It cannot interface with the target sensor as a Slave.

元の投稿で解決策を見る

1 返信
1,520件の閲覧回数
ckphua
NXP Employee
NXP Employee

The SPIFI interface can only be used a Master only. It cannot interface with the target sensor as a Slave.