About the Emulator in LPCXpresso_v8.2.2.650

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About the Emulator in LPCXpresso_v8.2.2.650

3,079 Views
TakMa
Contributor I

Windows10にIDEというタイトルをインストールし、エミュレータ
LPC11U35_QuickStartBoard(Embedded_Artists)としてインストールしました0244_lpc11u35_ssci1114_0x0000.bin上記のファイルを
インストールして、LPC1114FN28用のエミュレータとして
使用します。
使ってみましたが、認識されません。

数年前にWindowsXPにLPCXpresso_6.1.0.164をインストールした状態で、
Debug_Configurations、上記のボードをエミュレータの一種として設定し、
DAP-Linkとして認識した記憶があります。

LPCXpressoに特別な設定が必要ですか?

0 Kudos
Reply
6 Replies

2,894 Views
TakMa
Contributor I

I will buy MCU-LINK and see if LPCXpresso recognizes it or not. If there is a problem with my confirmation, please help me again. I'll close this question. Thank you for your support.

0 Kudos
Reply

2,958 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi TakMa 

Sorry we can't understand Japanese. Could you please edit your question to English? Thanks a lot.

Have a nice day,

Jun Zhang

0 Kudos
Reply

2,954 Views
TakMa
Contributor I

About the Emulator in LPCXpresso_v8.2.2.650

I installed the title IDE on Windows10 and as Emulator
LPC11U35_QuickStartBoard(Embedded_Artists),
0244_lpc11u35_ssci1114_0x0000.bin
Install the above file and use it as EmuLator for LPC1114FN28.
I tried using it, but it doesn't recognize it.

With LPCXpresso_6.1.0.164 installed on WindowsXp several years ago,
In Debug_Configurations, set the above board as a type of Emulator,
I remember recognizing it as DAP-Link.

Do I need any special settings for LPCXpresso?

0 Kudos
Reply

2,943 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi TakMa 

This board LPC11U35_QuickStartBoard(Embedded_Artists) is not NXP product and we can't help you test it.

I suggest you checking its usage on the website or  with Embedded_Artists support.

https://www.embeddedartists.com/products/lpc11u35-quickstart/

Thanks,

Jun Zhang

0 Kudos
Reply

2,936 Views
TakMa
Contributor I

Now, as the Emulator in LPCXpresso_v8.2.2.650
Please tell me which boards are available.

 

0 Kudos
Reply

2,923 Views
ZhangJennie
NXP TechSupport
NXP TechSupport
0 Kudos
Reply