AOAA PWM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AOAA PWM

1,147件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jim android on Mon Mar 04 02:34:18 MST 2013
Hello everyone. Im a beginner programmer and starting from scratch. Im doing some small development with the embedded artists AOAA board which has the LPC1769 processor. I got the examples up and running and i was told this is the forum i should post on. I want to control a simple servo motor with PWM using an external port on the AOAA board. Im using LPCXpresso and the lpc link to program the AOAA board.I dont know where to go from here as every example seems to be re directing me to the Arduino development which has its own servo library.

Any help or any direction anyone could point me in would be a huge help as the AOAA boards development seems to be scarce.

Thank you
ラベル(1)
0 件の賞賛
返信
0 返答(返信)