AN12327SW dualbootloader

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AN12327SW dualbootloader

1,408件の閲覧回数
zhangeh10594
Contributor III

In AN12327SW‘s  folder ,when I was double click the post_build_mdk.bat,and it caused an error,like this :

pastedImage_2.png

Incorrect image signature.I don't know why this mistake happened,so I want to ask you how to solve this problem.

And after that ,I continue with the instructions above for AN12327.Probably because of the mistake above,when I was excuting  the file of flash_program.bat,it also causes a mistake like this.

ERROR:UartPeripheral() can not open PC UART port (COM4) ,speed(57600hz).

I believe this mistake was caused by the mistake above。So I want to know how to solve the problem above, thank you very much!

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,316件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

Which bin file do you work with? can you please test the original dsbl_app.bin file under the AN?

Have a nice day,

Jun Zhang

0 件の賞賛
返信