AES encryption using AN11241

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

AES encryption using AN11241

1,766 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by terrype on Sun Aug 10 22:29:53 MST 2014
Hi Guys,  I try to build the AN11241 in LPC Expresso board with LPC expresso and getting error that _ROR() is undeclare. 
Is it some think like key function in Keil ?
标签 (1)
0 项奖励
回复
2 回复数

1,596 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by terrype on Mon Aug 11 16:53:02 MST 2014
Thanks guys.  I thought it was part of Keil compiler command and re-write the function, it is working now. Thanks

terry
0 项奖励
回复

1,596 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Aug 11 00:23:14 MST 2014
_ROR() is provided by the CMSIS "core_cmInstr.h" file. This should get pulled in if you link against either the CMSIS-CORE library project for the part you are using, or else with the LPCOpen libraries. Please see the LPCXpresso User Guide for more details.

Regards,
LPCXpresso Support
0 项奖励
回复