ADD out of spec

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ADD out of spec

882 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by williamjsell on Sat Feb 20 13:55:59 MST 2016
We are using the lpc11u68 device.  Using a function generator generating a triangle wave to test the adc, we see an ~8 count jump every 400 counts or so..  The spec indicates the transfer curve should be between 2-3 counts.  We tested two parts with the same performance.  So the adc performance is down to 2^9 with this 8 count error.  Not very good; anyone else seen this performance?
标签 (1)
0 项奖励
回复
2 回复数

870 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by starblue on Sun Feb 28 08:36:21 MST 2016
I would guess something is wrong in your setup (e.g. bad input signal, bad timing), but your description is rather vague.
I've done static measurements with 10-bit ADCs in other controllers, and they were quite good.
0 项奖励
回复

870 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by williamjsell on Sat Feb 27 15:15:05 MST 2016
Anyone, or am I the only one who thinks the ADC in this processor is lousy?
0 项奖励
回复