ADC2,3,4 CHANNEL ADDRESS NEED

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADC2,3,4 CHANNEL ADDRESS NEED

4,397 Views
aravindpb5009
Contributor III

HAI 

 i am using lpc824  in IDE adc header file having only for adc0 address only i need all channels address. i searched but didn't got plz let me know the address of all channels address  plz find my  below attachment of ADC0 address 

Labels (1)
0 Kudos
Reply
4 Replies

4,315 Views
carstengroen
Senior Contributor II

You need to read the documentation. This is not how the ADC works. There is 1 ADC converter, ADC0.

This has a number of inputs that can be selected

Datasheet:

pastedImage_2.png

Users Guide:

pastedImage_1.png

0 Kudos
Reply

4,316 Views
aravindpb5009
Contributor III

ok

0 Kudos
Reply

4,316 Views
soledad
NXP Employee
NXP Employee

Hi, 

You can use MCUXpresso SDK and use the ADC examples as reference. 

You can download it from the next link: 

https://mcuxpresso.nxp.com/en/welcome

pastedImage_1.png


Have a great day,
Sol

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

4,316 Views
aravindpb5009
Contributor III

thanks for your asisitances

0 Kudos
Reply