ADC pins permanently grounded in LPC2368

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ADC pins permanently grounded in LPC2368

738 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ramana on Thu Nov 27 23:29:53 MST 2014
       I'm using 6 ADC channels of lpc2368 to measure currents in my project. The issue is, I have been facing regular failures of ADC channels over long run. After some days at site, the ADC readings are becomes 0, when I debug the hardware, i have observed that, some of the ADC input pins of LPC2368 are showing short to Gnd of Controller.
    
      The circuit block diagram is in the attachment. It has been a big problem to me, need to replace the controller every time when the failure is observed. Please suggest me how can I prevent these failures.

Every suggestion is appreciable.

Thanks in advance


      
     
      
标签 (1)
0 项奖励
回复
2 回复数

718 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ramana on Fri Nov 28 20:49:27 MST 2014
ok, Thank u.

0 项奖励
回复

718 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Fri Nov 28 02:18:36 MST 2014
My suggestion. Don't double post!
0 项奖励
回复