ADC input as wake up source

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC input as wake up source

1,754件の閲覧回数
vineethhegde
Contributor II

Hi,

Please let me know, whether kinetis and LPC micro-controller has ADC input as wake-up source from deep sleep mode(Low power mode).

 

Regards,

Vineeth

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,535件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Vineeth113 754,

   It determined by which mode and chip you are using.

  1. the kinetis chip:

pastedImage_1.png

  As you know, the stop and VLPS can be waked up by the interrupt, then you just need to check whether the ADC module can work or not in the according low power mode.

  pastedImage_2.png

pastedImage_3.png

So, if the ADC can work in the according low power mode, and that low power mode can be waked up by the interrupt, then enable the ADC interrupt, after the conversion is finished, the interrupt happens will wake up the according mode.

2. LPC chip

  Take LPC5411x as an example.

pastedImage_4.png

No ADC wake up in the deep sleep mode.

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信