ADC input as wake up source

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ADC input as wake up source

1,334 次查看
vineethhegde
Contributor II

Hi,

Please let me know, whether kinetis and LPC micro-controller has ADC input as wake-up source from deep sleep mode(Low power mode).

 

Regards,

Vineeth

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,115 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Vineeth113 754,

   It determined by which mode and chip you are using.

  1. the kinetis chip:

pastedImage_1.png

  As you know, the stop and VLPS can be waked up by the interrupt, then you just need to check whether the ADC module can work or not in the according low power mode.

  pastedImage_2.png

pastedImage_3.png

So, if the ADC can work in the according low power mode, and that low power mode can be waked up by the interrupt, then enable the ADC interrupt, after the conversion is finished, the interrupt happens will wake up the according mode.

2. LPC chip

  Take LPC5411x as an example.

pastedImage_4.png

No ADC wake up in the deep sleep mode.

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复