ADC conversion clock cycles

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC conversion clock cycles

2,391件の閲覧回数
TEMCEFF
Contributor IV

Hi, 

I got a small doubt. In LPC1768/69 ADC is SAR type. for a 12 bit resolution, it should take 12 cycles for complete conversion. But in user manual mentioned that,

A non-burst mode conversion requires
65 clocks and a burst mode conversion requires 64 clocks. 

Can you explain this?

Regards,

Muralidhar.

ラベル(4)
0 件の賞賛
返信
2 返答(返信)

2,274件の閲覧回数
TEMCEFF
Contributor IV

Anyone can help me on this.

0 件の賞賛
返信

2,274件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Avinash,

Regarding your question that the ADC conversion time of LPC17xx requires 64 clock cycles based on SAR mechanism, it is said that the ADC converter of LPC17xx is initial version, for the later ADC converter for example the ADC of LPC54xxx, the ADC is optimized, the ADC clock frequency becomes higher, the conversion time becomes shorter.

BR

Xiangjun Rong

0 件の賞賛
返信