ADC configuration for ADC1_7 pin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC configuration for ADC1_7 pin

804件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LPC_beginner on Sun Jun 23 04:30:32 MST 2013

I am very new to LPC43xx series processors. My problem is with reading ADC  using a specific channel.


After going thorough the user guide and examples provided, I have come up with following steps.


 /* get scu base  */
 p = (LPC_SCU_Type*)(LPC_SCU_BASE);
 


 /*


  *  Select ADC function


  */
 p->ENAIO1 |= 0x80; //Enable ADC function for  ADC1_7 (pad PF_7 in BGA256 package)


 /*
  * Disable internal pullup  
  * Disable internal pull down 
  * Select  function  as GPIO
  */
   p->SFSPF_7 = 0x14; // Is this configuration is correct??
 
   
 /* Set GPIO as input mode */
 GPIO_SetDir(GPIO_PORT_7,(1<< 21), INPUT_MODE);
 
 /* disable band gap option */
  p->ENAIO2 = 0;


 /* ADC initialize */
  ADC_Init(LPC_ADC1, 200000, 10); /* Initialize ADC1 */
 /* Disable ADC Interrupt * 
 ADC_IntConfig(LPC_ADC1,ADC_ADINTEN7,DISABLE);


 ADC_ChannelCmd(LPC_ADC1,ADC_CHANNEL_7,ENABLE);
 ADC_StartCmd(LPC_ADC1,ADC_START_NOW);
  /*


   * Wait for conversion to complete


   */
  while (!(ADC_ChannelGetStatus(LPC_ADC1,ADC_CHANNEL_7,ADC_DATA_DONE)));
  ADC_val = ADC_ChannelGetData(LPC_ADC0,ADC_CHANNEL_7);


}


I have measured the pad PF_2  which is having voltage of 1.56, but  I always get 0 in adc register.


Verified that  DONE bit is getting set after the adc conversion start.


Do I missed any initialization.


Appreciate any pointers on this issue...


ラベル(1)
0 件の賞賛
返信
0 返答(返信)