ADC channels in LPC54606J512BD100

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADC channels in LPC54606J512BD100

Jump to solution
1,602 Views
prasannanaik
Contributor III

Hi,

   I want to know the actual number of ADC channels available in LPC54606J512BD100. While refereing to user manual i could see that ADC7 to ADC10 are not available in 100 pin products. So only 8 ADC channels are available in LPC54606J512BD100?

Of these 8 ADC lines, 3 have been multiplexed with SWD interface, so only 5 channels are available in LPC54606J512BD100 right?

Thanks and best regards,

Prasanna

Labels (1)
0 Kudos
Reply
1 Solution
1,533 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Prasanna,

The SWO pin of SWD can choose PIO0_8, so I think we can use 6 channels .

pastedImage_1.png


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

1 Reply
1,534 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Prasanna,

The SWO pin of SWD can choose PIO0_8, so I think we can use 6 channels .

pastedImage_1.png


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------