ADC LOWPRIO bit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC LOWPRIO bit

1,928件の閲覧回数
ianbenton
Senior Contributor I

Could you please clarify the action of the LOWPRIO bit in the SEQA_CTRL register.

The manual says that it sets the priority for sequence A.

In low priority mode, any SEQB trigger is ignored  - thus SEQA has higher priority.

In high priority mode, the SEQB trigger interrupts the SEQA sequence, and the SEQA sequence has to wait until the SEQB sequence is completed before it can resume - thus SEQA has lower priority.

This seems completely contradictory to the description.

Please advise.

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

1,839件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Ian Benton ,

I also think the name "Low priority" "High priority" may be misunderstood.

While the real function of this bit please refer to the clarify:

pastedImage_1.png

Hope it helps,


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

1,839件の閲覧回数
ianbenton
Senior Contributor I

Are you going to correct the manual?

0 件の賞賛
返信

1,839件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Lan,

I will report it document team, while I'm not sure whether it will be changed .

BR

Alice

0 件の賞賛
返信