A question about MCUXpresso Config Tools

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

A question about MCUXpresso Config Tools

3,143 Views
afzhang
Contributor I

Our company used LPC54016JET100 chip.I have a problem that I used MCUXpresso Config Tools,but it does not contain LPC54016JET100.Which type do i choose in MCUXpresso Config Tools?

Labels (4)
0 Kudos
Reply
2 Replies

3,001 Views
soledad
NXP Employee
NXP Employee

Hi, 

Please follow the bellow steps, 

1. Select "Create a new standalon ..." and click Next 

pastedImage_1.png

2. Select LPC54000 -> LPC54016,  on "Select processor package" select the device you need, 

pastedImage_2.png

Have a great day,
Sol

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

3,001 Views
afzhang
Contributor I

Hi,

Thanks!

B/R

Aifei Zhang

发件人: soledad

发送时间: 2019年6月27日 22:39

收件人: Aifei Zhang

主题: Re: - Re: A question about MCUXpresso Config Tools

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: A question about MCUXpresso Config Tools

reply from soledad <https://community.nxp.com/people/soledad?et=watches.email.thread> in LPC Microcontrollers - View the full discussion <https://community.nxp.com/message/1170716?commentID=1170716&et=watches.email.thread#comment-1170716>

0 Kudos
Reply