A minor RTC defect at the example of LPCUSBlib_MassStorageHost in LPCOpen 2.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

A minor RTC defect at the example of LPCUSBlib_MassStorageHost in LPCOpen 2.1

1,455 Views
jeremyhsiao
Contributor II

In the example of LPCUSBlib_MassStorageHost in LPCOpen 2.1 for LPC1769, it seems that there is a minor code defect at setting RTC (time will be used in FAT32).

 

int rtc_initialize (void)
{
...
Chip_RTC_SetFullAlarmTime(LPC_RTC, &rtcTime);

...

}

 

It should be

 

int rtc_initialize (void)
{
...
Chip_RTC_SetFullTime(LPC_RTC, &rtcTime);

...

}

Besides, this function also seems to contain defect (but it is not called in example code):

int rtc_settime (const RTC *rtc)
{
RTC_TIME_T rtcTime;

rtcTime.time[RTC_TIMETYPE_SECOND] = rtc->sec;
rtcTime.time[RTC_TIMETYPE_MINUTE] = rtc->min;
rtcTime.time[RTC_TIMETYPE_HOUR] = rtc->hour;
rtcTime.time[RTC_TIMETYPE_DAYOFMONTH] = rtc->wday;
rtcTime.time[RTC_TIMETYPE_DAYOFMONTH] = rtc->mday;
rtcTime.time[RTC_TIMETYPE_MONTH] = rtc->month;
rtcTime.time[RTC_TIMETYPE_YEAR] = rtc->year;

Chip_RTC_GetFullTime(LPC_RTC, &rtcTime);

return 1;
}

It should be:

int rtc_settime (const RTC *rtc)
{
RTC_TIME_T rtcTime;

rtcTime.time[RTC_TIMETYPE_SECOND] = rtc->sec;
rtcTime.time[RTC_TIMETYPE_MINUTE] = rtc->min;
rtcTime.time[RTC_TIMETYPE_HOUR] = rtc->hour;
rtcTime.time[RTC_TIMETYPE_DAYOFMONTH] = rtc->wday;
rtcTime.time[RTC_TIMETYPE_DAYOFMONTH] = rtc->mday;
rtcTime.time[RTC_TIMETYPE_MONTH] = rtc->month;
rtcTime.time[RTC_TIMETYPE_YEAR] = rtc->year;

Chip_RTC_SetFullTime(LPC_RTC, &rtcTime);

return 1;
}

Labels (3)
0 Kudos
Reply
1 Reply

1,301 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Jeremy Hsiao,

Thanks for your sharing, and I'll report the suggestion after I confirm it.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply