4370 USB Device NON ROM Examples Wanted.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

4370 USB Device NON ROM Examples Wanted.

1,704 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Wed Mar 11 19:56:55 MST 2015
Does anyone have links to 4370 USB (0) device examples, especially HID or CDC, that DO NOT use the ROM API?

Preferably for LPCXPresso (rather than Keil/IAR) and preferably using LPCOpen (rather than CMSIS).

Thanks in advance for any links you may have to share.

Regards, Mike
Labels (1)
0 Kudos
Reply
3 Replies

1,691 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Thu Mar 26 09:58:03 MST 2015
I have certainly seen the previous release -- 0.97.

Does this have 4370 (I.e. High Speed) targets.

Also, this seems quite old (2012-11-09 23:15) and CMSIS based.

But thank you.

Mike
0 Kudos
Reply

1,691 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Thu Mar 26 08:35:52 MST 2015
Hi Mike,
Not sure, if you already looked at
http://www.lpcware.com/content/nxpfile/nxpusblib-v098

0 Kudos
Reply

1,691 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Thu Mar 26 06:20:25 MST 2015

Quote: MikeSimmonds
Does anyone have links to 4370 USB (0) device examples, especially HID or CDC, that DO NOT use the ROM API?

Preferably for LPCXPresso (rather than Keil/IAR) and preferably using LPCOpen (rather than CMSIS).

Thanks in advance for any links you may have to share.

Regards, Mike



Anyone out there?
0 Kudos
Reply