24BIT RGB Signals in Datasheet

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

24BIT RGB Signals in Datasheet

1,301 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by RandyM on Thu Apr 25 11:14:26 MST 2013

For the LPC435x, on page 131 of the LPC435x datasheet, the LCD panel connection table for TFT seems off.  For blue bits [2:7] there are no "pin used" assignments.  I'm going to hope that this is a type-o and the obvious choices for pins were just accidently not filled in.  Can anyone verify?

Labels (1)
0 Kudos
Reply
1 Reply

1,267 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Wouter on Fri Apr 26 03:01:32 MST 2013

Hi Randy,


 


Thanks for pointing this out! Indeed it's just a typo, nothing to worry about. I'll submit an UM/DS update request.


The obvious choices are indeed the right one, so PB_0, PB_1, PB_2, PB_3, P7_1 and P7_2 should be used for BLUE7..BLUE2


 


Regards,


Wouter

0 Kudos
Reply