2 LPC1768 SPI master slave

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2 LPC1768 SPI master slave

2,749件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Rahul mankumbare on Fri Jan 15 06:25:52 MST 2016
Hi,

I want to use LPC1768 as a master & other LPC1768 as a slave in SPI.

I am using code bundle eg

In first LPC 1768 I am using master program & in second I am using slave program.

But it gives verify error as a output.

As in example code of Slave clock is generated . Why it is required when master clock pin is given to slave clock pin.
ラベル(1)
0 件の賞賛
返信
0 返答(返信)