1549 Software Reset

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1549 Software Reset

2,218件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by celephicus on Thu Sep 11 02:54:45 MST 2014
Has anyone had success with the NVIC_SystemReset() function to performa software reset on the 1549? I have some code that works perfectly on the LPC1114 but it locks up with a hard fault after the reset.\ on the LPC1549. This is my first project with the M3 so I have some learning to do I think :)
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,919件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Thu Sep 11 16:29:50 MST 2014
Hi celephicus,
It works. I have just tested it on Keil MCB1500 board which contains LPC1549JBD100 (http://www.keil.com/mcb1500/). I used Keil tool chain.
0 件の賞賛
返信

1,919件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Thu Sep 11 03:16:45 MST 2014

Quote: celephicus
Has anyone had success with the NVIC_SystemReset() function to performa software reset on the 1549?



No problems since March, no idea what you are doing...
0 件の賞賛
返信