12-bit ADC – a mistake in the LPC4370 datasheet documentation (Rev. 2.3)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

12-bit ADC – a mistake in the LPC4370 datasheet documentation (Rev. 2.3)

1,055 次查看
przemyslawbejta
Contributor I

There is an incorrect equation (4) of op amp’s output voltage in the chapter: 13.9.3 Non-inverting single-ended circuit for input 0 V to 3.3 V (page 147).

At the moment we have the following equation:

     Vout = Vcom * R1 / (R1 + R2)

but it should be:

     Vout = Vcom * R1 / (R1 + R2) + Vin_pos * R2 / (R1 + R2)

标签 (1)
0 项奖励
回复
1 回复

848 次查看
soledad
NXP Employee
NXP Employee

Hi,

I will inform this to our documentation team. Thank you for your feedback.

Have a nice day!


Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复