12 VDC motor speed and direction control using GPIO and Timer interrupt using current sensor with LPC1768

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

12 VDC motor speed and direction control using GPIO and Timer interrupt using current sensor with LPC1768

907件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ravindra on Mon Apr 27 11:03:19 MST 2015
Hello Together,

I have uploaded few files related to 12VDC motor control. create the project and build to get the hex file. Bin file is not generated.

I have used the LPC1768 board from NGX technoloigies for code validation.

Thanks
Ravindra

Original Attachment has been moved to: src.rar

ラベル(1)
0 件の賞賛
返信
0 返答(返信)