11Exx libraries

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

11Exx libraries

2,540 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ronkrem on Sun Dec 15 16:31:34 MST 2013
In setting up to develop an LPC11Exx application in LPCXpresso, we find there are two core libraries available: CMSIS_CORE_LPC11Exx and CMSIS_v2p10_LPC11Exx.

Which library is recommended by NXP?

Regards, Ron
标签 (1)
0 项奖励
回复
3 回复数

2,471 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ronkrem on Sun Dec 15 18:18:22 MST 2013
Many thanks.
0 项奖励
回复

2,471 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Sun Dec 15 16:56:38 MST 2013

Quote: ronkrem
In setting up to develop an LPC11Exx application in LPCXpresso, we find there are two core libraries available: CMSIS_CORE_LPC11Exx and CMSIS_v2p10_LPC11Exx.



CMSIS_CORE_LPC11Exx version is CMSIS V3.2 and therefore the newer version....
0 项奖励
回复

2,471 次查看
accelmotion
Contributor III

Where are these core libraries located? I can't find them in my LPCXPresso 8.2.2 directories. Are they from some external source?

0 项奖励
回复