1 - wire protocol Example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1 - wire protocol Example

3,886 Views
shaheenshamshad
Contributor III

Hi

I am trying to interface one wire protocol chip with LPC54618 MCU using mcuXpresso IDE and sdk 2.4 version.

I tried to find an example from sdk example section but I did not get any.

Kindly guide.

Regards

SS

Labels (1)
0 Kudos
Reply
3 Replies

3,613 Views
shaheenshamshad
Contributor III

Is there support people to guide?

I want to interface ds18b20 temp sensor.

0 Kudos
Reply

3,613 Views
BlackNight
NXP Employee
NXP Employee

There is a Processor Expert component for Kinetis (but not LPC) here: McuOnEclipse Components: 09-July-2017 Release | MCU on Eclipse 

An example project is available on GitHub: mcuoneclipse/Examples/KDS/tinyK20/tinyK20_1Wire at master · ErichStyger/mcuoneclipse · GitHub 

I hope this helps,

Erich

0 Kudos
Reply

3,613 Views
soledad
NXP Employee
NXP Employee

Hi, 

Unfortunately, there is no example like you need. 

Please check the following thread as a reference. 

https://community.nxp.com/thread/453861

Have a nice day!

Sol

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply