Peripheral reinitialization after waking-up from Power Down mode for LPC55S69

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Peripheral reinitialization after waking-up from Power Down mode for LPC55S69

Peripheral reinitialization after waking-up from Power Down mode for LPC55S69

The documentation is only valid for the LPC55xx and LPC55Sxx families. In power down mode, some of peripherals for LPC55xx are power off, which means that the peripherals lose it’s power in power-down mode, so it is required to reinitialize the peripherals after waking-up from  power down mode. The DOC lists the peripherals which lose power in power down mode and are required to initialize, introduces the procedure to enter the power down mode, and  the procedure to reinitialize the peripherals after waking-up from power down mode.

The doc is attached and power scheme is also attached.

添付
100%が役に立ったと言っています (1/1)
バージョン履歴
最終更新日:
‎07-20-2020 01:25 AM
更新者: