What is the maximum display resolution that emWin can support?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the maximum display resolution that emWin can support?

3,295件の閲覧回数
lpcware-support
Senior Contributor I

The maximum display resolution is limited by the LCD controller, the CPU bandwidth, the buffers, and the external bus speeds, as well as the panel size, the color depth and the refresh rates. Use the LCD Controller Bandwidth calculator on LPCware.com to determine your LCD parameters.

  • LPC247x bus bandwidth calculator
  • LPC178x and LPC40xx bus bandwidth calculator
  • LPC18xx and LPC43xx bus bandwidth calculator
ラベル(2)
タグ(2)
0 件の賞賛
返信
0 返答(返信)