What is the maximum display resolution that emWin can support?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What is the maximum display resolution that emWin can support?

2,551 次查看
lpcware-support
Senior Contributor I

The maximum display resolution is limited by the LCD controller, the CPU bandwidth, the buffers, and the external bus speeds, as well as the panel size, the color depth and the refresh rates. Use the LCD Controller Bandwidth calculator on LPCware.com to determine your LCD parameters.

  • LPC247x bus bandwidth calculator
  • LPC178x and LPC40xx bus bandwidth calculator
  • LPC18xx and LPC43xx bus bandwidth calculator
标签 (2)
标记 (2)
0 项奖励
回复
0 回复数