The CAN controller goes into bus off mode when my application tries to send a CAN message. There is no activity on the CAN bus. Why?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The CAN controller goes into bus off mode when my application tries to send a CAN message. There is no activity on the CAN bus. Why?

5,054 Views
lpcware
NXP Employee
NXP Employee

There are many causes of this and all relate to an issue between the CAN controller and the bus. For example no CAN transceiver, CAN transceiver disabled, broken connection between the CAN_L/H pins and the CAN controller.

"FAQ contribution from Embedded Systems Academy, experts in CAN bus. For more information visit www.esacademy.com"

Labels (1)
Tags (1)
0 Kudos
Reply
0 Replies